Part Number: OPA462
Hello E2E Experts,
I would like to design constant current source with this specifications:
output current (peak-peak) = 10mA;
Frequency range = 1Hz -100kHz
Load = 10 ohm- 4800 ohm (resistive load)
I tried to design the source according to known equations, but unfortunately, I’m having issues with the bandwidth. I thought adding preamplifiers at the input would help, but unfortunately, it didn’t. So I’d like to ask if there’s anyone who could please help me?
I’ve attached the circuit diagram.