Part Number: USB2ANY
Other Parts Discussed in Thread: BQ79600EVM, , BQ79600-Q1
Dear TI support staff,
I am currently attempting to Communicate with a BQ79718EVM using the BQ79600EVM as the bridge device. The GUI Tool works without any issue.
the Connection layout is: PC -> USB2ANY (FW 3.1.1.14) -> BQ79600EVM -> BQ79718EVM
Communicating with the USB2ANY works fine (calling the USB2ANY.dll ver. 2.8.2.0). However attempting to communicate with the BQ79600EVM fails - presumably due to UART baudrate incompability. The USB2ANY 2.8.2.0 API Reference (USB2ANY API Specification ) lists the max baud rate configurable at 230400 bps while the BQ79600EVM Documentation (BQ79600-Q1 Evaluation Module User's Guide (Rev. B) ) lists the EVM's Baudrate at 1Mbps.
Trying to use the firmware version 3.1.1.14 on the USB2ANY causes the u2a_Open function call to throw an error and ask for a downgrade to firmware version 2.8.2.0.
This leads me to an impasse where i cannot find a viable way to communicate via UART with the BQ79600EVM.
My questions regarding this are:
- How can i achieve UART communication with the BQ79600EVM via USB2ANY sucessfully? Is there a dll for 3.1.1.14 or am i missing something else entirely?
Thank you very much for your help in this matter.
With best regards,
Florian Bahn