Part Number: XTR300
Hi,
I want to use XTR300 to test and set it to the current output mode. I set the Rset and Ros to 1K, the input is 2.027V and 1.014V. But the output is (3.207~3.232) and (-2.940~-2.950), which is not stable and not following the transfer function, I think it is strange and I want to know the reason. Thanks in advance.
Figure for the ouput, red is the voltage between a 300ohms resistor(load), blue is the input. 
Best,
Sam