I believe, but I'm not certain, that this schematics is wrong for the TRF37D73:

- The operating frequency is 1.5 GHz, while the 33nH inductor SRF is 1.7 GHz (LQP03HQ33NH02D). The LQP03HQ33NH02D is rated for 150 mA while the TRF requires 50 mA. Is that ok?
- Is it acceptable to have a ferrite in the line (the thinking was to reduce noise further), but it's probably dumb as it might lead to issues?
- I assume the feedthrough capacitor is ok.
Thanks!