AMC1350-Q1: Technical inquiry request regarding TI isolation amplifier (AMC1350-Q1)

Part Number: AMC1350-Q1


■ Target Product
TI Isolated Amplifier / AMC1350-Q1

■ Inquiry Content
1. I would like to connect the secondary side (OUTP, OUTN) to a single-ended input circuit (ADC input of a general-purpose microcontroller). Do you have any recommended circuits?
2. I would like to share the power supply with the microcontroller, so I must connect GND2 to OUTN. Is this acceptable?
(I tested this on an evaluation board and confirmed that the offset is approximately 1.4V and the gain is approximately 0.2.)