This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2356-EP: Decoupling Capacitance

Part Number: OPA2356-EP

I have designed a circuit using the OPA2356-EP, with 100nF decoupling capacitance as suggested in power supply recommendations on page 19 of the datasheet. However I notice that page 20 lists 10uF as the minimum decoupling capacitance, which seems quite large. There is a 10uF back at the regulator, but each opamp only has 100nF locally.

The fundamental of my signal is 20 MHz, the 100nF provides very low impedance at that frequency, but there are also some higher frequency harmonics that I would like to preserve if I can. I am seeing slightly worse slew rate than expected on the output signal. I am therefore wondering if something like 22nF decoupling for high frequency signal and 10uF for bulk at each opamp would be a more suitable arrangement, but given the conflicting information in the datasheet I wondered if you could give any insight on the intended/preferred decoupling arrangement before I start trying things empirically!

Thanks

  • Hello Brett,

      The way you have it is correct. We usually place a small value capacitor (10nF to 100nF) as close as possible to the supply pins of the amplifier and we place the larger value capacitor (1uF to 10uF) closer to the supplies. Datasheet should have been more clear and mention the 10uF to be an addition (closer to your regulator) to the previous page's suggestion of 0.1uF (closer to the amplifier). 

      For the slew rate comment, do you happen to have an output capacitor as your load or lower input voltage (maybe not pushing amplifier to its max). We recently released this app note on slew rate: www.ti.com/.../sboa610.pdf

    Thank you!
    Sima