Part Number: LM358B
Other Parts Discussed in Thread: OPA994, LM358
Hi team,
Question 1
The datasheet for LM358BIPWR includes an item on capacitive load driving capability, which is listed as 100pF. Customer understand that if a capacitive load greater than 100pF is connected to the LM358BIPWR, the phase margin in the feedback will decrease, increasing the risk of oscillation.
On the other hand, phase margin correlates with frequency, and I believe that if the actual operating conditions are DC or very low frequency, the risk would tend to be lower even if a large capacitive load is connected to the LM358BIPWR.
Is this understanding correct?
Question 2
Could you please recommend some operational amplifiers that don't have limitations on capacitive load driving capability? I'm considering using them as a voltage follower for a DC+1.65V power supply.
Question 3
Customer is concerned about phase margin when external noise is applied and is considering whether they can measure this in-house. Does TI conduct measurements that include external noise? If you have any insights, I would appreciate your guidance on measurement conditions and methods.
Best regards,
Hayashi