Part Number: AMC3301
Other Parts Discussed in Thread: AMC1200, AMC3302, OPA365
Hi Team,
Posting on behalf of our customer.
Would it be feasible to transmit the differential output of the AMC3301 (AMC1200 also applies) over a 12"-24" twisted pair 100-ohm ribbon cable ? The receiving end would be an instrumentation amplifier to convert it to single-ended for an ADC. The datasheet doesn't appear to say much about the amplifier's stability. Would it make sense to add series resistors (10-50 ohm) on the AMC3301's output lines before sending over the cable? I obviously won't be able to add a termination resistor at the INA's input because the AMC3301 wouldn't be able to drive the necessary current for that anyway. The application will be a SiC-based motor inverter separated from the controller by this ribbon cable.
Or would you recommend some sort of analog line driver to accomplish this? But I hate to add the extra parts though.
Regards,
Danilo