Other Parts Discussed in Thread: TLC3702, LM2903
Hi,
I am planning to use TLC3702 comparator in replacement of a LM2903 without modifying the output pull-up.
So when the output will be low, there will be a current of 15V / 1.5kOhm = 10 mA that will flow in the output MOS transistor.
Does this device accept this current in its "recommended operating parameters" ?
Also, another parameter that I do not understand is "Max Input current": as it is a very high input impedance device, what is the meaning of this parameter set to +/- 5mA?
Regards