Part Number: OPA192
Other Parts Discussed in Thread: OPA2675, OPA1678, OPA2189, OPA2375, OPA2182, OPA2192, OPA211
Dear Team,
Case1)
please can you propose a replacment for LT1028 in regards to the output voltage noise?
In orginal desing the LT1028 is followed by LT1210 to support curretn spikes ( we will repleace the LT1210 with OPA2675)
Both LT1028 and LT1210 are confugured in unity gain configuration and are supplied with +4V and -3.3V, but we can also use +5V/-5V or +2.5V/-2.5V as we need to supply a -0.7V BIAS, I can share more info in DM.
Case2)
We need to generate a low noise BIAS of 3.5V ( Average cuurent 1mA) and ripple < 30uVpp, voltage of the opamp +5.2V / 0V
-----------------------------
i did some sorting and OPA1678, OPA2375, OPA2189, OPA2182 and OPA2192 looks promising,
Please let me know your toughts.
Best Regards,
d.