Part Number: TLV9020
I understand that the TLV9020 has fault tolerant inputs that can handle being powered when the part does not have power. What is the worst case input current on these inputs under this condition?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV9020
I understand that the TLV9020 has fault tolerant inputs that can handle being powered when the part does not have power. What is the worst case input current on these inputs under this condition?
Thank you.
Hello John,
Yes. See the second paragraph of section 6.4.2.2
"The fault tolerant inputs can be any value between 0V and 5.5V, even while V+ is zero or ramping up or down.
This feature avoids power sequencing issues as long as the input voltage range and supply voltage are within
the specified ranges. This is possible since the inputs are not clamped to V+ and the input current maintains the
value even when a higher voltage is applied to the inputs."
Currents are similar to the regular bias current (reversed biased junctions). See the graph figure 5-6 (~1-2nA).