Part Number: AMC0311S
Hello Experts,
I have a question regarding AMC0311S. The datasheet states in Table 7.1, 'Device Operational Modes,' that if the high-side supply is missing, the OUT pin should be driven to the VREF level. In my application, this is not working.
If the high-side supply fails and there is a 0.4V offset voltage at the VREF pin, the voltage at the OUT pin is only approximately 60 mV. Low Side supply is stable at 5.1V, Power supply pins are buffered with 100n and 1µ as recommended in datasheet. The circuitry is the same as your Typical Application example in the datasheet, except of REFIN Pin is driven to 0.4V.
During normal operation (with the high-side supply present), the 0.4V offset is applied correctly.
Are there any known topics regarding this behaviour?
Best regards!
Moritz Nüßlein