Part Number: TAS2563
Hello
I've got a question regarding the TAS2563 Characterization using PPC3:
You have to set the Thermal Limit parameter which is described as the difference between the maximum temperature of the speaker and the ambient temperature.
My speaker has a maximum temperature of 70°C.
Which temperature is used for the ambient temperature?
- Is the ambient temperature during characterization (in my case roomtemperature 25°C)
- Or is it the maximum amient temperature of the device i later use the speaker in. (in my case the
device is specified to run up to 65°C ambient temperature)
Thank you for your help and best regards
David