Hi
I am implemention I -V conversion i.e from 4-20mA to 0-5 V , for this i used RCV420 . But with the same IC can I convert 4-20mA to either 0-3V or 0-3.3V.
Pl help in this regard.
yours
Pavan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am implemention I -V conversion i.e from 4-20mA to 0-5 V , for this i used RCV420 . But with the same IC can I convert 4-20mA to either 0-3V or 0-3.3V.
Pl help in this regard.
yours
Pavan
Pavan,
The datasheet offers a method of using resistors in parallel with the input to reduce the gain of the circuit (see Figure 2). However, in your case, reducing the gain this much will cause relatively large offsets at low current levels. That being said I would agree with the above suggestion of adding a resistor divider and using an opamp in a unity-gain configuration to buffer the output signal.