Part Number: OPA2990
Dear TI,
I'm designing a driver circuit for driving a pair of MOSFET switches for switching a long communication line or cable between two power supply rails (36 V and 24 V). Currently the topology I'm working on consists of a dedicated gate driver IC and two N-channel switching transistors. For more details on the drive circuit, please see my previous discussion topic: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1581266/ucc21520-driving-long-cables
The high switching speed of the gate driver IC causes lots of oscillations when driving long cables at high speeds (2.4+ kHz). I have measured up to 46 V peak voltages seen by the load.
I think the solution to the oscillation problem would be to use a suitably slower switching speed. Based on some simulations, an op-amp (such as OPA2990) slewing the gate voltage of a complementary pair of FETs between ca. 16V and 42V in a controlled "ramp" of ~100 µs should help with the oscillation. The sketch below shows op-amps scaling the 0/5V input signal up to 15..45V suitable for driving the gates of common-source N-/P-FETs. Op-amps are powered from +48V and +12V rails. "Scope" trace below shows the input signal and the oscillating output voltage.

Which kind of circuit would you recommend to achieve this kind of output voltage slope from an op-amp? So far I've found TIDU026 and SBOA218B, but they seem to concern with slower slew rates up to 1s. Given a "step input" into an OPAx990, how to slow down its output slewing between 15V and 45 V in, say, ~100 usec (or about 0.3V/µs)?
Looking forward to your suggestions.