Part Number: OPA320
Other Parts Discussed in Thread: TINA-TI
Hi Sir/Madam,
This is Vishaal working as an Hardware Engineer. We are planning to use OPA320 as error amplifier which the Feedback is from rectifier output as 700V DC which should be pulled down to 2V to 3V and the Ref voltage will be from 2V to 3V which is also a DC. So, it would be helpful for us if you can send the reference Circuit for OPA320 in error amplifier configuration as soon as possible which can be used for the above mentioned application.
Thanks,
Vishaal S