This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1300B-Q1: Part num clarification needed

Part Number: AMC1300B-Q1
Other Parts Discussed in Thread: AMC131M03, AMC0311S

Good day to you

 

We have a requirement for V2L application. We need an Isolated AC voltage sense( 85V to 250V AC, 50Hz) and current sense -max current through the AC switch is 16A. 

 

Do you have any Isolator IC which have both AC voltage and current sense and it provides equivalent voltage in analog and current limit setting pin 16A.

 

We need to simple enable logic pin to control the AC switch.( no SPI)

 

  • Hello, 

    unfortunately we do not have a device that would do the both, voltage and current measurement. The only part that is remotely close to a multi-channel device is AMC131M03 and alternatives from this family. However, these require SPI and MCU configuration.

    If you wanted to build it discretely, then we have a new family of single-ended output isolated amplifiers (e.g. AMC0311s). You would need to add isolated power and external comparator. 

    Best regards, 

    Jiri Panacek,

    Systems Applications Engineer, 

    Isolated Converters