Part Number: USB2ANY
Hello,
I am trying to create my own application to communicate with the BQ97600EVM-030.
As a basis I am using the C# Example from the USB2ANY SDK.
To wake up the BQ97600 I have to send a "Wake Tone".
E.g.:
u2a.GPIO_WritePort(6, 1); /* Set GPIO 6 to low level - CS */
u2a.GPIO_WritePulse(4, 0, 2750); /* Output low level pulse on MISO line for 2,75ms */
u2a.GPIO_WritePort(6, 2); /* Set GPIO 6 to high level - CS */
Unfortunatley the execution time of the function calls are very slow.
Time between setting CS low and sending the low pulse on the MISO line is ~50ms.
Time after the pulse until CS high is again ~50ms.
Is there a way to improve the performance?
Thanks,
André Meyer