Part Number: THS4551
Other Parts Discussed in Thread: ADS127L01, ADS127L01EVM
To input the load cell output to the ADS127L01, I am using a THS4551 to amplify the differential signal. (I used the ADSL127L01EVM.)
The load cell specifications are a 5V power supply voltage, a rated output of 1mV/V, and a gain of 100x for the amplifier circuit. The ADC and op amp share a common ground, and the load cell output is input directly to the amplifier circuit without any level shifting.
When the load cell is powered at 5V, the differential voltage input to the ADC is approximately 3V, and the op amp output appears to be stuck to the rails. Compared to ground, AINP and AINN are approximately 2.5V. On the other hand, when the load cell is powered from the evaluation board's 3.3V power source, the differential voltage relative to ground is approximately 1.5V, and the system operates without any problems.
Regarding this phenomenon, is it correct to understand that the differential voltage input to the amplifier circuit does not need to be particularly concerned about the voltage relative to the ADC's ground? Also, I'm wondering why there's no problem when the voltage relative to GND is 1.5V, but the problem occurs when supplying 5V. Please check.
Thank you.