Part Number: INA826
Hi Teams,
The customer is currently using the INA826AIDR operational amplifier and has discovered an issue. According to the design in the diagram, the amplification factor should be changed to 150.7. However, it has been found that two chips have been replaced at the same position on the same PCB, and the amplification factors of the two chips are not quite the same, one is 149 and the other is 148. May I ask if this is an inherent error of the chips?