This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549: OPA549

Part Number: OPA549

Hi Dennis,

I need to build a circuit using an OPA549 to replace a servo amplifier that uses an EM-1803, without changing the motor. Firstly, since the OPA549 has only one output, I think a BTL configuration with two OPA549s is necessary. Also, the EM-1803 output generates a 15V DC offset, which the module creates automatically. I need help determining how to apply this DC offset. I can send the schematic of my current EM-1803 circuit.