Part Number: TPA2039D1
Hi BU,
My customer is using TPA2039D1 in the gaming chair application to create haptic feedback for his product.
In the second figure, the original value of C171 (corresponds to C286) = 0.1uF, C169 (corresponds to C284) and C52 (corresponds to C285) = 68nF. Customer has just updated the values like what are shown in second figure.

The input is a PWM signal.

After the first and second RC filter, it will have a 50Hz signal.

However, after passing through C171 = 0.1uF, the signal became like below, causing the haptic driving could not work.
Help needed:
- Can you help to check if there is anything incorrect of component placement at the input side?
- Can you help to check if there is anything incorrect for input signal just before entering VIP pin?
Thank you!

Regards,
John