Part Number: AMC1302
Other Parts Discussed in Thread: TMCS1126
Hi,
Our requirement is to perform bidirectional current sensing of +/- 30A.
We're planning to go with two approaches:
- Shunt + Isolation amplifier (AMC1302) + Differential Amplifier (TLV9000)
- Hall sensor (TMCS1126)
We have a system requirement that when the MCU goes into the standby mode, the board current consumption should be reduced to 0.5mA.
So far in the checked parts, I couldn't find EN/SHUTDOWN pin which would make the IC consume less current (selected ICs consume currents around 14mA).
Kindly suggest options & guide us in this regard.
Best Regards,
Prahaladh S