Part Number: AMC3330
Other Parts Discussed in Thread: TLV6001
Hi team,
My customer is considering designing an insulation‑resistance measurement circuit based on TIDA‑010232. I have three questions regarding this.
Since the input voltage to the AMC3330 will have the positive side at a higher potential, we are considering setting the VREF of the TLV6001 to a value lower than 2.5 V.
-
If the internal reference is set to 2.048 V, is it acceptable to apply 5 V to REFP and REFN? Or should these pins be left open when using the internal reference?
-
The voltage applied to ADIN is expected to be 0–5 V. Will the device operate properly even though the internal reference is 2.048 V?
-
We are considering a single‑ended configuration, with AIN0 connected to the analog input and AIN1 connected to the analog ground. My understanding is that using a differential input improves analog accuracy. Is this correct?
Best regards,
Kyohei