Part Number: INA181
I am trying to simulate a circuit with an INA181 current sense IC.
I have boiled it down to this circuit:

And I just pulled the spice model today.
When Vs1 is 0V (i.e., shorted to ground) I get this:

Note the time delay in the output, VF2. By adding a 50mV offset to Vs1, we get this:

Where everything lines up nicely.
I assume this has to do with:
"The linear range of the output stage is limited by how close the output voltage can approach ground under zero input conditions. In unidirectional applications where measuring very low input currents is desirable, bias the REF pin to a convenient value above 50 mV to get the output into the linear range of the device." from 7.4.2 of the data sheet, but I see nothing about how long it takes to recover from non-linear to linear range. 25 ms seems a bit excessive.
So is this just a SPICE artifact or actual device behaviour. Is there anyway to correct this without putting a voltage on the ref pin?