This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3113D2: Required Audio amplifire

Part Number: TPA3113D2
Other Parts Discussed in Thread: TPA3138D2

Dear  Team,
 
 We are currently working on an access control system project and require suitable amplifire and speakers that meet the following specifications:
 
- Sound pressure levels: 93 dB and 97 dB
- Audible range: Clearly audible from a maximum distance of 5 feet 
- IP65 rating for dust and water protection
- Industrial temperature range: -40°C to +85°C
 
 Can You suggest the Audio best Suitable Audio amplifire IC