This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA855: Regarding Input and Output

Part Number: PGA855

Dear Team, 

I came across this PGA849RGTR part which does Differential to Single ended Conversion with Variable gain controlled digitally. I am Planning to use this part in my design.

The below mentioned are my requirements, Please confirm that this part can be used.
I want Variable gain Controlled digitally, 
BW is 10Hz to 10MHz
Differential to Single ended Conversion.

One more question is I also want a part to do the same in opposite. 
I want the same process but Single ended to Differential. 

I came across this part PGA855 which is a Diff to diff. Can i use this for Single ended to Differential COnversion and have all the same features as it is in PGA849RGTR .

Looking forward to your response, 

Thank you and best regards, 
Maharajan P