I am looking at the LT1013I or LT1013AI. I am fine with the input offset voltage of the LT1013I but if the LT1013AI isn’t much more expensive I would use that part. I can’t seem to find either one on the TI website. Or if they have an equivalent part that would be alright as well. As of now I am looking at using the LT1013DID. The TI website states the part is -40C to 85C but the data sheet says the “I” suffix should be a -40C to 105C. Which is correct?
-Jason