Part Number: LM2917-N
Hi
The many permutations and design options for the LM2917 leave me unsure we have the design right. I wanted feedback if the circuit is correct.
Requirement:
fan tachometer output - need to trigger indicator (1/0) whether fan tach output is above or below 300Hz
two of these to be input to a logic circuit to drive bi-lvel LED - green if both OK, RED if EITHER is below 300Hz
1) We assumed "speed switch" for figure 18 in the datasheet was the simplest approach with minimal parts - is this correct?
2) We adjusted some part values for the frequency and voltage relevant.
3) we fed the output at collector with pullup to a NOR
is the choice of 2917/2907/8 pin/14 pin correct?
is the schematic correct?
are the values correct?
thanks
Pinhas