Part Number: OPA858DSGEVM
Hi,
We have a customer who ordered evaluation board OPA858DSGEVM from Mouser.
They have reported the following issues:
"The appearance of the device is complete and defect free, but the gain
should be 7 times. Currently, the laboratory has measured that it is only
1 time. We use a waveform generator to give IN+a 20mV, 1MHz sine wave. The
input and output (IN+and OUT) waveforms are exactly the same, with no
change in amplitude, indicating that the gain is only 1."
Could you please advise if there is a way they can test or trouble-shoot this board?
Kind regards
Thomas Rosendahl
Mouser Electronics
S/O 504429