Part Number: OPA355
OPA355 datasheet mentioned GBW = 200MHz at G=10 but as per graph in page13 Gain at 10v/v is ~ 15MHz can u explain me where i am wrong 

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA355
OPA355 datasheet mentioned GBW = 200MHz at G=10 but as per graph in page13 Gain at 10v/v is ~ 15MHz can u explain me where i am wrong 

Sruthi,
As per datasheet the GBW at G=10 is around 200Mhz, that corrosponds to -3dB bandwidth of around 20Mhz.
This is similar to the datasheet plot of gain vs frequency plot (Figure 18). Gain of 10V/v corrosponse to 20dB. Here in the plot also the gain is 3dB below the set gain of 20dB (or 10V/V) at 20Mhz.
Regards
Anant