Other Parts Discussed in Thread: TLC393, TLC339, TLC193, TLC372, TLC139
1. I have an application where I have to drive N-channel MOSFET depending upon signal from MSP430.Since MSP430 alone cannot drive the FETS, So I have put to op-amp between MSP430 & FETS. If conditions arises, MSP430 will drive op-amp, which will further drive FETS.
2. My circuit is battery operated & need to be very low current consuming.
3. Will Rail to Rail or open -drain serve this purpose. As I think with a voltage signal at op-amp input from MSP430, op-amp o/p can be driven to rails. Kindly suggest me the same.
4. Supply range: 7- 18V
5. High signal from MSP430 =3.0V, & Low signal=0.0V.
Regards,
Deepak