Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA141U

Hi,

Can someone advice if the INA141UA is compatiable with INA141U ?

I'm currently ussing the INA141U and was offering by the supplier to use INA141UA.

I want to make sure these two are identical.

Thanks,

Eli

  • Eli,

    The difference between the two versions is that the INA141U is the higher-grade version compared to the INA141UA. Specifications that are different between the two parts can be found in the corresponding columns in the datasheet:

    Notice that for many parameters, a typical value is not specified but rather a max value for the UA version of the part. I should also note that the "U" portion of the name is the package designation, SOIC -8 in this case, therefore the INA141U and the INA141UA have the same physical dimensions and pinout.

    Hope this helps!