Part Number: INA240A
Other Parts Discussed in Thread: TPS717
Hello team,
We noticed when the two REF input pins are tied together and the IC is placed on PCB with 3v3 applied the REF inputs are floating 1v65 with no connections to an external reference.
Seemingly the internal REF circuit does not require any external voltage when the two REF1/2 pins have been tied together. This observation contradicts the datasheet notes on how the REF inputs need an external bias voltage.
Are we actually adding noise into the amplifier by connecting an noisy 20KHz extern DAC to the REF1/2 inputs when they are already at 1v65 bias level? Do we actually need to force 1v65 bias on REF1/2 pins when they are on same PCB with 3 amplifiers REF1/2 inputs tied together via copper traces? Can we just leave the REF1/2 tied pins floating at 1v65 or will the bias follow the input/s signal?
Thanks in advance for investigating this very strange observation!