This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3110D2: Unable to see outputs on amplifier.

Part Number: TPA3110D2

I've tried troubleshooting this schematic of mine and am unable to find the error. I've measure the voltages around the IC and see that all PVCC are at 12V AVCC is also 12V. I initially  had SD and fault tied together with a pull up to 12V but now have SD floating so I can control it with a wire soldered to the pad either going to 0 or 12V. Fault is remaining high and not entering an error state.  I power my board with SD to ground and then move it to 12V and still Fault is High. GVDD is about 6.96V and is connected to PLimit. GAIN 0 and 1 are tied to GND and PBTL is also tied to ground. I have measured the input to make sure there are signals going to the inputs and there are. But fors ome reason the outputs are not working and the voltage on the OUT pins are around 2V which is a but suspicious. I have looked around for shorts and there are non. c9ea7215-10f7-4277-916d-5f39cb22c7f3.png