Part Number: TLV4H390-SEP
Other Parts Discussed in Thread: TLV4H290-SEP, TLV9024
Hello, I'm interested in powering the TLV4H390-SEP with 1.8V(V+) and 0V (V-)
In the data sheet www.ti.com/.../tlv4h390-sep.pdf, the common mode input range is listed as (V-)-0.2 to (V+)-1.5. Could you confirm that this actually means that the common mode range would be -0.2V up to 0.3V?
I can see on other forum posts for this part that a possible commercial equivalent is www.ti.com/.../tlv9024.pdfThis part seems to have a common mode input range of (V-)-0.2 to (V+)+0.2 - so I believe this would give me -0.2V to 2V.
Does the TLV4h390 data sheet have a typo?
I plan on using this part as part of an over current detection circuit so likely I'll just bias one input at a reference level and the other pin would be proportional to the current I'm measuring. Mostly want to figure out what level to bias one of the comparator input pins at. Half supply (0.9V) would probably be my start point. The data sheet however seems to hint that I'd need to bias at 0.2V maybe.
On a slightly different topic if I were to use the TLV4H290-SEP isntead, I could power at 3.3V or 5V. Which I guess would greatly increase the common-mode range. Would the part be happy having a pull up on its open drain outputs to 1.8V? Can the propagation speed of the TLV4H290 be improved by using stronger pull ups e.g 1k?
Appreciate the help!
Adam