Part Number: INA241A-Q1
Other Parts Discussed in Thread: AMC1351-Q1, OPA2188, INA241A, TLV387
Hello E2E Experts,
I have several elementary questions about offset voltage in a current-sense amplifier:
Question 1: If I compensate the offset voltage of an amplifier, can I expect it to remain compensated forever (for years)? (assuming the offset voltage drift is zero)?
Question 2: In the following circuit, if I compensate the offset voltage, can I expect Vout to always be proportional to the current flowing through Rshunt (assuming negligible offset voltage drift and common-mode voltage effects)?. Suppose Vref = 2.5V and Vcc = 5V (op. amp.)
Question 3: Can the offset voltage have a different value when the amplifier's input signal is a DC signal than when the input signal is an AC signal?
Question 4: Can the value of the offset voltage of an amplifier change over time or does it only change with temperature?
Regards,
TICSC