This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA125: INA125 - offseting the input

Part Number: INA125

Dear Sir,

 

I am designing load cell amplifier using INA125, where I need to measure very little voltage changes (whole volt span is within 1 mV). This works well up to Rg=30R, where Vout is approx. 2.50 V. 

However if I increase gain (lower RG), V out goes above my ADC range as well as doesn't respond normal to load cell changes anymore. Is there a way to offset this, so I could increase gain while keep Vout lower?

Supply is 12 V, Vref 10 V is used to supply the cell.

 

Best regards,

Gregor MACEK