This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: INA240 Gain Characteristics at Vs = 3.3 V

Part Number: INA240

The electrical characteristics table for this part specifies

Gain Error of 0.05% nominal, 0.20% max when the condition GND + 50 mV ≤ VOUT ≤ VS – 200 mV is met.

This table is specified to TA=25C, VS=5V.

Does the gain error change for a VS=3.3V part? When VS=3.3 VDC does the Gain Error of 0.20% hold.

  • Hello Julia, 

    Thank you for your post. 

    The specified max gain error at room temperature only applies to the 5V supply voltage condition. 

    That being said, you should see comparable error at 3.3V if you adhere to the linear range of the output of GND + 50 mV ≤ VOUT ≤ VS – 200 mV.

    I hope this helps, 

    Joe