Part Number: ISO122
Other Parts Discussed in Thread: ISO124, AMC0211S, AMC1411, ISO224, AMC1400, AMC3330
In a noisy industrial application i have a 4-20 ma and a -10 to +10 signal coming from sensors. I need to get these signals in a microproccesor and want to isolate these signals from the microprocesor. I found the ISO122/ISO124 and they look like they would work easily but was wondering as they are 30 year old technology if i would be better off going with something newer for better temperature and stability performance and also future availability of parts. I couldnt find anything that would handle the +/- 10 volt directly but wondered if i could scale and level shift with a OP amp to get a 0 to 2 volt signal and feed that into something like a AMC0211S. What advice would you give. I dont know the temperature range right now but i have a email into my customer now waiting for a answer but i know its not going to be room temperature and will vary.