Part Number: INA241A
Hi,
NC pin(pin4) of INA241A is descrived to connect to ground on D/S page2.
But in INA241AEVM , pin4 is leave floating.
Which one is recommended?
Regards,
Go
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Go,
Thank you for your post.
My Recommendation: Connect Pin 4 to Ground
The datasheet recommendation is the one to follow. Connect pin 4 (NC) to ground for your production design.
The datasheet is clear: pin 4 is classified as a "Ground" type pin with the description "Reserved. Connect to ground." [1]. This is reinforced by the recommended PCB layout (Figure 8-3), which shows pin 4 connected via a via to the ground plane [2], and by TI's reference design schematic, which also ties it to GND [3].
Why the EVM Differs (and Why It Still Works)
A TI engineer directly addressed this discrepancy and confirmed that leaving pin 4 floating poses no operational risk — in fact, the EVM designer intentionally left it unconnected [4]. The reason it works either way is that pin 4 has a weak internal pull-down resistor, so it self-biases to ground even when floating [5].
That said, externally grounding it is best practice because it provides improved noise immunity by fixing the potential externally rather than relying on the weak internal pull-down.
Bottom Line
For a standard design with GND at 0V, ground pin 4 per the datasheet. The EVM's floating pin is acceptable but not the recommended practice for production designs.
I hope this helps,
Joe