Part Number: INA241A
Hi,
Would it be possible to receive further design support via private messaging, since I am not allowed to disclose details publicly?
The design is based on the following E2E thread:
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1490146/ina240-current-sensing-amplifiers---general-questions/5724690
with the following additional features:
-
- High‑side current measurement
- Wide measurement range from 0 A up to tens of amperes
-
Resolution in the hundreds of µA or a few mA
- Dual‑range sensing using two sense resistors (Rsense) and an MOSFET
- Adjustable overcurrent detection
Best regards
Josko