Part Number: INA4230
I would like to confirm whether INA4230 can be used for sensing bidirectional motor current.
- Device: INA4230
- Application: Motor current sensing
- The motor rotates in both directions, so the current direction through the shunt resistor reverses depending on rotation.
When the motor current reverses, the polarity across the shunt resistor also reverses.
In this condition:
- Can INA4230 still be used as a current-sense amplifier?
- Is it acceptable if the polarity between IN+ and IN− is reversed due to current direction?
- Are there any functional limitations or accuracy concerns when IN+ becomes lower than IN−?
Shota