Part Number: OPA855
Other Parts Discussed in Thread: OPA695
Hi TI Support Team,
I am currently working on an optical receiver design and observing a very specific, non-linear saturation behavior on my signal chain. I would like to get your insights on whether this is a known characteristic of the OPA855's internal architecture when subjected to extreme input overdrive.
System Overview:
-
Sensor: Avalanche Photodiode (APD) receiving 1 ns optical pulses from a laser.
-
1st Stage (TIA): OPA855 with a feedback resistor Rf = 4 kOhms.
-
2nd Stage: OPA695 configured in an inverting amplifier setup with a gain of 2.
-
Measurement: The attached graph shows the peak output voltage measured at the end of the chain (after the OPA695) as a function of the peak optical power of the laser.
Observed Behavior:
As shown in the attached plot, as the optical power increases, the system exhibits a "double saturation" profile with an intermediate voltage drop:

-
Linear Region & 1st Saturation: The output rises linearly until it hits a first saturation point at roughly 2.5V.
-
The "Sag" / Voltage Drop: As optical power continues to increase, the saturated output voltage suddenly drops by approximately 0.4V (down to ~2.1V).
-
2nd Saturation (Hard Clamping): At even higher optical powers, the voltage recovers and hard-clamps back up to 2.5V+.
Questions:
-
Can you confirm if this specific "sag" during deep input overdrive is a known behavior of the OPA855 caused by the activation of internal input protection diodes?
-
Does the internal clamping mechanism temporarily alter the biasing of the output stage, leading to this voltage drop before feedforward takes over?
-
Reliability: Are there any long-term reliability concerns for the OPA855 when repeatedly subjected to this deep overdrive state with 1 ns pulses?
-
Do you recommend any external protection schemes (e.g., external clamping diodes on the input) to mitigate this without sacrificing the bandwidth required for 1 ns pulses?
Thank you in advance for your time and expertise!
Best regards,
Florian Bonnet--Galand - IRIDESENSE