Part Number: INA310B
I use the INA310 in a somewhat dynamic configuration, where the sense resistor could temporarily be floating w.r.t. the VS supply and GND. However, when I then connect a voltmeter between either the IN+ or IN- pin and GND, I measure a -0.5V on either pin, suggesting that a curreent flows from GND into the IN+ or IN- pin. Applying a current meter between IN+ or IN- and GND confirms that, as this gives a ~70uA current into the INA310 pins. This seems rather strange, as the device is powered by +12V on VS. Current now flowing into the INA310 implies that within the device a negative voltage has to be present to support this. Is this correct and why is it there, or is there another cause for this phenomenon?
Kind regards,
Cees van Teylingen