This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM101A-N: Date code mismatch LM101A MD8

Part Number: LM101A-N

Date code decode details required:

Material: LM101A MD8

Date code on COC: 2536+5

Date code on waffle: 59A53C1

How to decode date code 59A53C1.LM101A C OF C.pdf 

  • Hi Karthik,

    The code 59A53CI is the lot trace code for the device. The "5" indicates the year, 2025, and the "9" indicates the month it was created, in September (9). The remaining characters are for internal tracking of the device fabrication/assembly.

    From the date code, on COC, we can see that this matches, since 2536 corresponds to the 36th week in 2025, which is first week of September. The "+5" indicates it was the 5th lot built that week.

    Please let me know if you have further questions.

    Best regards,
    Carrie