Part Number: TAS2572EVM
Other Parts Discussed in Thread: TAS2572
hi,sir
we are unable to get ClassH mode working on TAS2572(smart PA,1s battery,VBAT=2.9V,L=1uH,8ohm load)
Symptom:
1.BST_CFG_02 (0x22) = 0x23 (Class-H) + any VBOOST_MAX_CTRL (tested 0x5B/6V and 0xA7/11V) → PVDD stays at VBAT level during 0dBFS playback
2.BST_CFG_02 (0x22) = 0xA3 (Always ON) → PVDD correctly ramps to target voltage
3.Firmware (tas2572RCA1.bin) loads successfully; audio playback works in Always ON mode
Our understanding from datasheet (Section 7.3.1.3.4):
Class-H requires CLASSH_TUNING_x[23:0] registers to be configured via PPC3 software based on system-level parameters (VBOOST_MAX, C_OUT, gain, BST_ILIM, inductor value).
are the default reset values of CLASSH_TUNING registers sufficient for Class-H to function with default VBOOST_MAX=0xA7?if not,can you provide the PPC3-generated CLASSH_TUNING values for our configuration: 1S, VBAT=3.9V, L=1µH, C_OUT=10µF, VBOOST_MAX=6V (0x5B), BST_ILIM=default,8ohm load?
- can you share PPC3 software access so we can generate these parameters ourselves?


the 7v is right?