Part Number: LMP2012QML-SP
As is common for OPAMPS, the datasheet of the LMP2012QML-SP specifies that the input voltage must not exceed the supplies (absolute max rating for differential and common mode input range).
However, i noticed that the absloute max ratings also specify a maximum current of 30mA at input pins. Does this limit reflect max. rating of clamping diodes at the input of this OPAMP? i.e. is the device safe even if the input voltage exceeds the supplies, provided that the current remains limited below 30mA?
kind regards,
Daniel