This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5802: TAS5802 Dynamic EQ

Part Number: TAS5802
Other Parts Discussed in Thread: TAS2563, TAS2781

Subject: TAS5802: How to implement continuous Dynamic EQ (DEQ) / Dynamic Bass Extension across the entire input range?

Description:
Hello TI Audio Experts,

We are currently designing a smart speaker system utilizing the TAS5802 digital input Class-D amplifier. To maximize acoustic performance while ensuring system reliability, we intend to implement a Continuous Dynamic EQ (DEQ) / Dynamic Bass Extension feature that automatically adjusts the low-frequency response based on the real-time input signal level (ranging from 0 dBFS down to -36 dBFS).

Our target specification includes 4 discrete operational milestones to illustrate the intended behavior:

  1. 0 dBFS Case (Speaker/Amp Protection): Low-frequency attenuation starting from 150 Hz with a -12 dB/oct slope to protect the speaker driver from over-excursion and prevent amplifier clipping at maximum volume.
  2. -12 dBFS Case (Bypass): No extra signal processing is applied; the signal passes through with a flat baseline response.
  3. -24 dBFS Case (Low-Level Bass Boost): Low-frequency boost begins at the speaker's native attenuation onset frequency (100 Hz) down to a target low frequency of 60 Hz, achieving a maximum boost of +12 dB relative to the baseline.
  4. -36 dBFS Case (Ultra-Low-Level Bass Boost): Low-frequency boost begins at 100 Hz down to a target low frequency of 30 Hz, achieving a maximum boost of +24 dB relative to the baseline.

The conceptual curve of this behavior is illustrated in Figure 1 below:

Dynamic_EQ_Concept.png

[Figure 1: Conceptual_DEQ_Target_Response.png]

Crucial Requirement: While these 4 levels define our primary milestones, the EQ adjustment must be completely continuous and dynamic across the entire 0 to -36 dBFS spectrum. The filter characteristics must smoothly interpolate in real-time according to the input level envelope, rather than step-switching discretely between static profiles.

Current Status & Verification:
We have consulted with TI Korea regarding this requirement. The local support team informed us that while the TAS5802 supports static EQ configuration shifts per discrete level, it lacks a native, hardware-driven continuous "Dynamic EQ" processing block in its DSP pipeline.

To prove the feasibility of the target acoustic target curves, we have already successfully tested and verified the individual biquad profiles on a 6-ohm dummy load at discrete levels. As shown in Figure 2, the individual curves for both the woofer and tweeter signal paths perform exactly as intended when programmed statically:

Dynamic_EQ_1.png

[Figure 2: Measured_Discrete_EQ_Results.png]

Since individual control works perfectly, we would like to get a review from the TI HQ Audio DSP Architecture team to see how we can bridge this gap into a fully continuous dynamic system.

Questions for TI HQ Experts:

  1. Is there any native, undocumented block or advanced component within the TAS5802 DSP architecture (or inside PurePath Console 3) that can facilitate a truly continuous, signal-dependent Dynamic EQ / Dynamic Bass Extension?
  2. Can this continuous adaptation be achieved by creatively configuring the built-in Automatic Gain Limiter (AGL) or Dynamic Range Compressor (DRC) blocks (e.g., using specific sub-band sidechain routing)?
  3. Alternatively, if we implement an external host MCU to perform real-time envelope detection and dynamically recalculate/write the Biquad filter coefficients via I2C at runtime, is the TAS5802 architecture capable of handling rapid, continuous coefficient updates? If so, what is the maximum recommended update frequency over I2C to avoid audio artifacts such as clicks, pops, or zipper noise?
  4. If the TAS5802 cannot support this continuous requirement, are there any alternative TI Smart Amp parts (e.g., TAS2563, TAS2781, or higher-tier TAS6x series) or application notes you recommend that support continuous Dynamic Bass Extension out-of-the-box?

We would highly appreciate a deep technical review and guidance on how to implement this system successfully.

Thank you.

HR Kim @Hanwha Vision

  • Hi Kim,

    We will investigate your questions and get back to you soon. Meanwhile, you could refer to attached apps notes for TAS5802 DSP processing. Thanks.TAS58xx tuning guide.pdf

  • Hi Kim.

    Sorry for waiting.

    1. Native Undocumented Dynamic EQ Block in TAS5802/PPC3

    Answer: No, there are no undocumented or hidden processing blocks in the TAS5802 DSP pipeline or PurePath Console 3 (PPC3) that can implement true continuous, signal-dependent Dynamic EQ (DEQ) / Dynamic Bass Extension.
    • The TAS5802 is a mid-range Class-D amplifier with a fixed, fully documented DSP pipeline. Its processing capabilities are limited to: static Biquad EQ (up to 10 bands per channel), Automatic Gain Limiter (AGL), Dynamic Range Compressor (DRC), volume control, and basic speaker protection.
    • TI does not ship products with unpublicized core processing features, and we cannot provide support for any non-documented functionality. The TAS5802 was not designed with a dedicated dynamic EQ hardware block, as this feature is reserved for our higher-tier smart amplifier families.
  • 2. Achieving Continuous Adaptation via Built-in AGL/DRC

    Answer: No, you cannot implement sub-band dynamic EQ by reconfiguring the built-in AGL or DRC blocks.
    • The AGL in the TAS5802 are full-band processing modules only. They can only adjust the gain of the entire audio spectrum, not selectively target the 150Hz and below low-frequency band that your design requires.
    • There is no internal routing mechanism to feed the AGL/DRC level detection output to the Biquad EQ blocks for adaptive adjustment. The AGL/DRC operate independently of the EQ pipeline.
    • While you could use AGL/DRC for full-band dynamic gain control, this would not deliver the frequency-specific bass boost/attenuation behavior you have specified.
  • Subject: Feasibility of Host-Software Based Dynamic EQ (DEQ) Implementation for TAS5802 via I2C

    Hi Peter Wu5,

    Following up on my previous inquiry, I understand that the TAS5802 does not have a built-in DSP block for sub-band Dynamic EQ (DEQ), and that the internal AGL/DRC cannot be routed to control the Biquad filters.

    To achieve our target bass management, we have implemented an external software-based DEQ control on our host processor. I would like to share our current implementation status and ask for your expert opinion on its feasibility and any potential hardware risks.

    System Overview (Host SW DEQ):

    • Audio Capture: Hooking into the ALSA PCM Playback callback (512 sample blocks, 48kHz, roughly 10.67ms per block).

    • Level Estimation: Continuously calculating Fast RMS, Slow RMS, Peak, and Crest Factor.

    • Control Logic (Attack/Release):

      • Attack (Gain Reduction): Evaluated over approx. 53.35ms for natural protection when loud signals are detected.

      • Release (Gain Increase): Evaluated over approx. 1053ms when returning to quieter segments.

    • EQ/Filter Updates:

      • For high levels (0dBFS to -6dBFS): Dynamically adjusting HPF cutoff frequency via LUT.

      • For lower levels (< -6dBFS): Using a combination of Base EQ (±3dB steps) and Fine EQ (±1dB steps) Biquad coefficients via LUT.

    • I2C Control: To prevent blocking the audio callback (which previously caused issues within the 10.67ms window), we decoupled the I2C writes using a delayed update thread. The Biquad coefficient updates are sent to the TAS5802 dynamically as the target state changes.

    We have successfully tested this and the spectrogram/level tracking results (tested with noise, sine, and speech ramps) look promising. However, before finalizing this architecture, we have a few questions:

    Questions:

    1. Continuous Biquad Updates: Are there any reliability or hardware lifecycle issues with continuously updating the TAS5802's Biquad registers via I2C during active playback at this frequency (e.g., changes triggered every 50ms ~ 1s depending on the audio material)?

    2. Audio Artifacts: Will updating the Biquad coefficients on the fly cause any internal DSP phase issues, clicking, or popping noises inside the TAS5802, even if we carefully handle step sizes and slew-limiting in our software?

    3. General Feedback: Is this host-based I2C dynamic control approach something you have seen successfully deployed with the TAS5802 (or similar families), or are there hidden pitfalls we should be aware of?

    Thank you for your guidance!

  • Hi Kim,

    I will need further investigation to answer your new questions one by one.

    1. Reliability & Hardware Lifecycle of Continuous Biquad Updates

    • No write wear risk: All TAS5802 control and Biquad registers are implemented in volatile SRAM, not flash or EEPROM. SRAM has an infinite number of write cycles—you could update the registers every 1ms continuously for the entire 10+ year lifespan of the product with no degradation to the device.
    • Your update rate is extremely conservative: Your 50ms to 1s update window is 10-200x slower than the maximum safe rate for the TAS5802. We have customers running updates as fast as 10ms (100Hz) in production with no issues, and for bass management applications, anything faster than 50ms is completely inaudible to the human ear.
    • Only two minor reliability risks to mitigate:
      1. I2C bus corruption: A corrupted I2C write can load an invalid Biquad coefficient, which may cause the DSP to output loud noise or lock up. Mitigate this by:
        • Enabling I2C ACK checking and retrying failed writes exactly once (more retries are unnecessary and can cause longer glitches)
        • Writing a full set of 5 coefficients per Biquad in a single I2C transaction, not individual bytes
      2. Updates during device state transitions: Never write Biquad coefficients while the TAS5802 is initializing, entering/exiting standby, or experiencing an under-voltage/over-temperature reset. Always confirm the device is in the PLAY state before sending any coefficient updates.
  • 2. Audio Artifacts: Phase Issues, Clicks & Pops

    Answer: With your current software implementation and the TAS5802's built-in hardware features, you will not experience any audible artifacts.
    • TAS5802 has native frame-synchronized smooth updates: This is the most important hardware feature that eliminates artifacts. When you write a Biquad coefficient, it is buffered internally and only applied at the start of the next audio frame (~20.8µs at 48kHz). There is no possibility of a mid-frame coefficient change, which is the root cause of hard clicks and phase glitches.
    • Phase shifts are completely inaudible: While changing Biquad coefficients does introduce small phase shifts, the human ear is completely insensitive to phase changes at frequencies below 200Hz. For your bass management use case (targeting <150Hz), phase performance is a non-issue and will not affect sound quality.
    • Edge case note: The only scenario where you might hear minor zipper noise is if you force a gain change faster than your 53ms attack time. Your current attack/release times are perfectly optimized for natural bass response, so this should never occur in normal operation.
  • 3. General Feedback & Hidden Production Pitfalls

    Answer: This exact host-based I2C dynamic control approach is widely and successfully deployed in mass production with the TAS5802 and all similar mid-tier TI Class-D amplifier families (TAS57xx, TAS56xx). However, there are 5 critical hidden pitfalls that teams often miss:
    1. I2C Bus Priority & Contention
      • You correctly decoupled I2C writes from the audio callback—this is the single most important best practice. However, ensure the I2C update thread has lower priority than the audio playback thread. If the I2C thread blocks the audio thread, you will experience audio dropouts, not just delayed EQ updates.
      • Avoid sharing the I2C bus connected to the TAS5802 with high-traffic devices (touchscreens, IMUs, sensors). Bus contention can cause delayed or corrupted coefficient writes. If possible, dedicate a separate I2C bus to the amplifier.
    2. LUT Coefficient Stability Validation
      • While you have tested your discrete curves, validate every single entry in your interpolation LUT on the TAS5802 across the full temperature (-40°C to 85°C) and voltage (3.0V to 5.5V) range. A single unstable Biquad coefficient (caused by rounding errors during interpolation) will cause the DSP to output full-scale noise, which can destroy speakers.
      • Never calculate Biquad coefficients on the fly in the host MCU. Always use pre-calculated, pre-validated LUTs as you are doing now.
    3. Device State Synchronization
      • If the TAS5802 ever resets (due to over-temperature, under-voltage, or ESD), it will revert to its default power-up EQ configuration. If your host MCU does not detect this reset and re-sync the current coefficients, you will get a sudden, potentially dangerous jump in volume.
      • Mitigation: Implement a 1-second heartbeat check that reads a known register from the TAS5802. If communication fails, re-initialize the device and re-apply the current EQ coefficients immediately.
    4. Internal AGL/DRC Interaction
      • If you have the TAS5802's built-in AGL or DRC enabled, your host DEQ bass boosts will increase the overall signal level seen by the AGL, causing it to engage earlier than expected and undo your bass boost.
      • Recommended: Disable the internal AGL and DRC entirely and implement all dynamic gain control in your host software. This gives you full control over the audio chain and eliminates conflicting gain adjustments.
    5. Thermal & Speaker Protection
      • Your +24dB bass boost at low volumes significantly increases power dissipation in both the TAS5802 and the speaker.
      • Mandatory test: Run the device at 40°C ambient with a -36dBFS 30Hz sine wave for 8 continuous hours. Confirm no thermal shutdown occurs and the speaker does not exceed its maximum temperature rating.