Part Number: INA333
Hi experts,
Need advice on this one.

The simulation shows straight line but when the circuit was built, the output showed a sawtooth waveform instead. What could be the issue?

More information:
1. The oscilloscope probe I used is standard lenght.
2. There are no long wires between the output point and the measurement terminal; the oscilloscope probe is connected to the output point via a 5 cm wire.
Regards,
Marvin